Skip navigation.
Our energy working for you.Our energy working for you.




Read Our Newsletters

Updates on our latest whitepapers, products and solutions.
Register here.

2008 News Releases

FOR IMMEDIATE RELEASE – 31 January, 2008
For further information, contact: Madeline Foss, 763–574–5942

Alberta Children’s Hospital designed for speedy recoveries and power reliability

Three 2 MW diesel generator sets from Cummins Power Generation provide standby power for Alberta Children's Hospital

Three 2 MW diesel generator sets from Cummins Power Generation provide standby power for Alberta Children’s Hospital.

– The bright, playful façade of Alberta Children’s Hospital in Calgary looks like a random stack of colored building blocks—and that’s how the kids who had a hand in its design wanted it to look. This colorful exterior represents the goal of the new hospital—responding to children’s needs. From the state–of–the–art medical facilities that aid patients’ recoveries to the standby power system that ensures their safety, the hospital’s vision is to reduce stress and promote healing in ways that are uniquely tailored to the children it serves. For the 3.5 MW electrical needs of the 133–bed, 750,000–square–foot hospital, officials chose Cummins Power Generation Inc. generators and controls.

With kids as customers, quality is the bottom line

During the early design stages of the hospital, which opened in September 2006, architects asked young patients what they thought a hospital for kids should look like. From these early concepts, the hospital is designed to be all about the children who go there for treatment. With a focus on family–centered care, the hospital includes sleeping facilities for parents in each patient room, a pet visitation room and healing gardens. However, most patients are treated on an outpatient basis and visit the hospital’s diagnosis, assessment and treatment clinics. This clinic–based program has been used as a worldwide model for outpatient care.

Building a hospital specifically for children drove and impacted every part of the design. “Everyone on the design and construction team agreed that intangible factors—not just price—were important, because it is a children’s hospital,” said Gerry Stebnicki, electrical design team leader with Stebnicki + Partners in Calgary. “This made the whole approach unique. We sent a request for proposal (RFP) to generator manufacturers stating our essential performance requirements rather than a complete design; all major components of the hospital were chosen that way. We chose Cummins Power Generation within that context, because they offered the best value of all the tendered proposals. Once they were chosen, they participated in the budget control and design decisions, working in concert with the rest of the group to make it happen. That’s a big reason why the project was so successful.”

Redundancy equals reliability

One example of the planning team’s quality–driven focus is the high reliability designed into the standby power system. The team created N+1 redundancy at all levels. “Although we initially recommended two 2 MW generators to serve the hospital’s 3.5 MW total load,” said Stebnicki, “hospital officials wanted to be able to run at full load even if one generator was down — so there are three generators.”

Separate power building offers benefits and challenges

The three generators ― Cummins Power Generation model DQKC ― are housed in a building 400 meters (1312 feet) away from the main building. This minimizes noise and vibration in the hospital, allows ground–level access to the generators in an emergency and simplified the design of the generator cooling system.

Because of the distance between the power building and the hospital, Stebnicki chose 4,160–volt supply lines to the hospital rather than the Canadian standard of 600 volts. “Increasing the voltage allowed us to deliver the same amount of power with smaller conductors,” he said. “We saved so much on the conductor costs that the overall standby system ultimately cost less.” The 4,160–volt lines run underground and then through a series of duct banks to the main building’s penthouse.  From there, power is stepped down to 347/600 volts.

The design team chose the PowerCommand® digital master control (DMC) system from Cummins Power Generation for two reasons: 1) complete integration with the generators; and 2) its ability to meet interoperability requirements. There are two touch–screen control panels for the generators and transfer system, one in the generator building and another in the penthouse. They are linked by fiber–optics. “The system can be controlled from either point — and changing anything on either screen updates the other screen in real–time,” said Steve Falk of Trotter & Morton, the project’s electrical construction manager. “It is also possible to control the system through a PC from anywhere, but the design team chose not to implement that capability, partly for security reasons and partly because qualified personnel are in the hospital at all times.”

According to Dave Drinkwater, the hospital’s maintenance and engineering manager, Calgary’s municipal power company, Enmax, is a highly reliable source of power. Outages are rare; in fact, there have been none since the hospital opened. ”In the rare event that Enmax needed to shed loads, we would be considered a high priority,” said Drinkwater.

System exceeds standards

The Canadian Standards Association’s Z–32–04 standard, ”Electrical Safety and Essential Electrical Systems in Health Care Facilities, ” requires that generators be online within 12 seconds of utility outage. The PowerCommand® system does much better than that, according to Stenicki. “The DMC has extensive capabilities. It enables operators to monitor all major loads in the building and provides history on the profiles of all those loads, which is a very effective planning tool. When the system detects a loss of normal voltage, the UPS takes over and can, theoretically, supply power for all critical needs for hours. But the UPS doesn’t have to supply power for that long; that isn’t necessary, because as soon as there’s a power outage, the system also sends a start signal to the generators.”

Once the generators are up to speed — which takes about 10 seconds — the system again transfers power smoothly to the generators. Then the system senses when the utility comes back online, and again makes a smooth, synchronous switch back to the utility power. Fuel capacity for the generators is 50,000 liters (13,208 US gallons); depending on loading and the season, the generators could power the entire hospital for approximately 44 hours.

In a simpler system with one standby generator, the move from one power source to another would be accomplished through a transfer switch. “But since the hospital is much more complex—three generators, UPS and feeds from two utility substations—there actually are no transfer switches,” said Stebnicki. “Switching is done through the main breakers; the DMC software accomplishes seamless, synchronous switching.”

The new hospital also exceeds other requirements of Z–32–04. For example, the standard lists critical loads that must be connected to the emergency power system. For an acute care facility such as Alberta Children’s Hospital, that list includes operating rooms, the intensive care unit, trauma care and emergency facilities, stairway lights and power outlets around every patient. The list also includes ventilation fans—in both the operating rooms and patient rooms—that determine airflow direction and therefore help to control the spread of infection. However, since just two of the three 2 MW standby generators are needed to handle the hospital’s entire load, it is unlikely that the hierarchical system will be called upon. Drinkwater’s staff tests the generators and associated equipment weekly using actual hospital loads rather than a load bank.

Interstitial floors for efficient maintenance

Another design element in Alberta Children’s Hospital that contributes to overall reliability is its interstitial floors: Every other floor is solely devoted to mechanical, electrical, telephone and plumbing equipment. Sealed, permanent conduits pass through each interstitial floor into the healthcare areas below. This contrasts greatly with the previous paradigm in which equipment was jammed into the space above a suspended ceiling. In Alberta Children’s Hospital, the interstitial floors are the same height as the healthcare floors, 14 feet, which provides more space to work in (and a floor to work on), so maintenance is faster and more efficient. More important, interstitial floors allow workers to “operate” on the building’s systems without interrupting or contaminating the vital healthcare activities occurring below.

With reliability and redundancy as their watch words, everyone on the Alberta Children’s Hospital design team — including Cummins Power Generation — has responded to problems with innovative solutions. But, then again, innovative solutions were the requirement, since the health — and often the lives — of children hang in the balance every day.

Cummins Power Generation, a subsidiary of Cummins Inc. (NYSE: CMI), is an industry leader in introducing advanced low–emissions power generation solutions around the world. With over 80 years’ experience, the company’s global distributor network delivers innovative, reliable and cost–effective solutions for any power need — commercial, industrial, recreational, emergency and residential. Products include alternators, generator–drive engines and temporary or permanent pre–integrated power systems, combining generator sets and power control and transfer technologies. Services range from system design, project management, financing, and operation and maintenance contracts to development of turnkey power plants. For more information, contact Madeline Foss, Cummins Power Generation, 1400 73rd Ave. NE, Minneapolis, MN 55432. Phone: 763–574–5942; fax: 763–574–5298.

©2009 Cummins Power Generation Inc. All Rights Reserved.